With pre-configured workstations for an individual solution
17 Jan 2022
The online configurator for GARANT GridLine workstations offers even more convenience. At the beginning of the session, the user can now choose whether he wants to build a workstation completely himself or adapt a basic configuration according to his wishes. GARANT workstations are available in three versions: mLevel for manual and eLevel for electric workstation height adjustment and eLevel+ with worktop height adjustment.
The provision of basic configurations considerably speeds up the online design of system workstations, because the user can immediately start the individual design without adding any basic components himself. Doing so, he has all the options to change and color-adapt the selected basic configuration and to supplement accessories. Accessories include, for example, support columns and perforated panels, support arms, energy and media rails, drawers and drawer casings for the base cabinet. The new "duplicate" functionality also allows the user to copy and save the current configuration to create variants. In the end, the planning precision improves and the users saves time. Get what you want – faster and easier!
The online configurator for GARANT GridLine workstations can be reached on www.hoffmann-group.com via the service area and the product pages for workstations. The tool allows the user to look at the workplace in 3D from all sides and get a realistic picture of the planned workstation. At the end of the session, the parts list can be displayed and a non-binding offer can be obtained from Hoffmann Group via the contact form.