![](https://www.hoffmann-group.com/media/media/_global/content/images/Sicherheitsschuh_690_w690.jpg)
Timeless design and a treat for the feet
10 Sept 2020
All feet are different. The first GARANT ‘comfort’ safety shoes offer excellent comfort for a whole working day. The light upper material made from resistant microfibre and the breathable inner lining gently adapt to the shape of the foot. To ensure that wider feet also feel comfortable in the shoes, the low shoes are available in two different widths. Insoles with weight-dependent shock absorption at the heels are available in three different thicknesses to reduce the strain on the knees and spine; and significantly contribute to a pain-free working day. Thanks to the new anti-slip sole GARANT comfort TPU with turning point, the shoes also provide extra sure-footedness. The shoes offer protection against electrostatic discharge (ESD) and are available in the four common safety classes S1, S1P, S2 and S3.
GARANT ‘comfort’ safety shoes combine high wearing comfort with a timeless, classic design. High-quality materials, a pinched manufacturing method and workmanship "Made in Germany" ensure the shoes’ weight is kept to a minimum yet they still offer great protection.
When the shoes were being designed, ergonomic requirements were constantly being taken into account to make them a valuable companion in everyday working life, and make a significant contribution to the long-term health of the wearer. The multi-width system allows the shoe to be adjusted to the width of the foot, and by replacing the insoles the cushioning can be adjusted exactly to the body weight of the wearer. Insoles are available in soft, medium and hard for a body weight of 50 to 120 kg. A perforation in the forefoot area of the insole ensures a high degree of air circulation and climate comfort. The models in safety classes S1 and S1P also have large ventilation slits in the upper material so that any excess body heat is dissipated quickly and the feet stay cool throughout the day.
The new GARANT ‘comfort’ safety shoes are available in sizes 36 to 48 and can be ordered from September 2020 via the eShop www.hoffmann-group.com or via the Hoffmann Group's catalogue 2020/2021.