![](https://www.hoffmann-group.com/media/media/_global/content/GARANT_Master_Gloves_Family_2021_690px_w690.jpg)
Equipped with twelve models against all dangers
8 Feb 2022
With its new protective gloves series ‚GARANT Master‘, the Hoffmann Group considerably facilitates the selection of multi-purpose and anti-cut gloves. The ten models of the new series, together with the two LABS-compliant silicone-free GARANT protective gloves, cover all risks associated with mechanical activities in dry, wet and oily environments. Many companies therefore only have to hold up to twelve models. This facilitates purchasing and creates space in the warehouse.
The new glove series ‚GARANT Master‘ meets the cut protection levels X/a to D with three models ‚GARANT Master fit multi-purpose gloves‘ and seven models ‚GARANT Master cut protective gloves‘. With their high-quality finish and ergonomic fit, the new protective gloves measure up to particularly high demands in terms of quality, protection and wearing comfort. The backing material used predominantly is 18-gauge fine-knitted fabric made of skin-friendly polyamide or nylon, elastane, lycra or special yarn. The special yarn makes it possible to dispense with skin-unfriendly glass or steel fibers even in higher cut protection levels such as C or D. Nitrile, nitrile foam and water-based polyurethane are used for the coatings and are optimized by finishing processes. The use of hazardous solvents such as DMF (dimethylformamide) is completely avoided.
The coatings make the gloves grippy, resistant and abrasion-resistant, yet allow maximum elasticity. This ensures a good tactile feel and a high level of fingerability, even when the coating is stronger. The result: A glove that is perfectly matched to its surroundings. In oily environments, the coating protects and provides a secure oil grip. In dry environments, for example, the GARANT Master fit glove also offers touch-screen capability.
The new protective gloves of the series ‚GARANT Master‘ can now be ordered in the eShop under www.hoffmann-group.com in sizes 6 to 12. The label ‚GARANT Master‘ stands for particularly high-quality products, which are characterized by very special properties.